Technical FAQs

Ask a Question

How is the ATV630 process drive setup for HMI start/stop and speed reference control?

Issue:
How is the ATV630 process drive setup for HMI start/stop and speed reference control?

Product Line:
Altivar ATV630 and ATV930 drives

Environment:
All 

Cause:
Normal control to be via HMI 

Resolution:
In the Complete Settings menu, select Command and Reference.
Set Ref Freq 1 Config = Ref Freq - Rmt Term
If the Control Mode = Not Sep, then the command channel will automatically be HMI and control setup is done.
If the Control Mode = Sep, then set Cmd Channel 1 = HMI.
Was this helpful?
What can we do to improve the information ?