Technical FAQs

Ask a Question

What drive product line will replace the ATV312?

Issue:
What drive product line will replace the ATV312?

Product Line:
Altivar 312 ATV312

Environment:
All models

Cause:
Transition to current product as ATV312 approaches obsolescence

Resolution:
The ATV320 drive is the recommended replacement to the ATV312.  See the attached file.
Was this helpful?
What can we do to improve the information ?