Technical FAQs

Ask a Question

Can Xanbus Cable be installed Underground for use with XW/XW+/CSW System?

Yes, but requires the use of proper outdoor/underground cables of the correct build and standard and is not to exceed the maximum length - Xanbus total 40m @ 250kbps.
Requires the use of Ethernet Cable designed for underground use. Can use CAT 5e or CAT 6 JELLY FILLED cable with correct outdoor rating and is compliant with local standards.
 
Was this helpful?
What can we do to improve the information ?