Technical FAQs

Ask a Question

How to clear F79 fault on MPPT80-600

Issue:
How to clear F79 fault on MPPT80-600

Product Line:
MPPT80-600 charge controller

Environment:
MPPT80 charge controller with fan over current fault

Cause:
Customer may try to clear faults with the clear faults option in the SCP.

Resolution:
F79 More than two Fan Errors have occurred within 30 seconds. The fan will cease operating, but the charge controller will continue operating though it will probably experience power derating. The fault will clear itself when the operator toggles power to the charge controller.
Was this helpful?
What can we do to improve the information ?