Technical FAQs

Ask a Question

For the SSRPTPDC25 what is the input consumption?

Issue:
Need to know the consumption of the solid state relay

Product Line:
SSR Solid State Relays

Environment:
North American Products

Cause:
Need to know the consumption of the solid state relay

Resolution:
The maximum input current consumption is 10mA at 32V
Was this helpful?
What can we do to improve the information ?