Technical FAQs

Ask a Question

ATV320 needs to set it for output contactor command and wire up the digital output for OCC.

Issue:
ATV320 needs to set it for output contactor command and wire up the digital output for OCC.

Product Line:
ATV312

Environment:
All

Cause:
Needs to use the digital output to control a relay for OCC.

Resolution:
Wiring goes as follows

Jumper +24vdc to DQ+  wire your + side of  you relay coil to DQ-  then wire the other side of the coil to Com

Program 
OCC in application menu to DO
Was this helpful?
What can we do to improve the information ?