Technical FAQs

Ask a Question

Can I charge my batteries to 100% while using the SoC stop trigger in the AGS?

Issue:
Can I charge my batteries to 100% while using the SoC stop trigger in the AGS?

Product Line:
Conext Series solar equipment and accessories
 
Environment:
Conext Series solar systems with both the Conext Battery Monitor and AGS connected
 
Resolution:
The maximum is 95% to protect the generator from situations where the battery is never detected as reaching 100%. There's unfortunately no way to combine start on SoC and stop on absorption exit. If you're certain that 95% won't be sufficient for your battery charging, then we recommend using Start DCV 30s and StopFloat for your triggers.

Cause:
Some batteries may not be fully charged at 95% SoC.
Was this helpful?
What can we do to improve the information ?