Technical FAQs

Ask a Question

Can the elbow fittings for the for the I-line II busway rated 200 - 600A be connected directly together?

Issue:
Can the elbow fittings for the for the I-line II busway rated 200 - 600A be connected directly together?

Product Line:
Busway

Environment:
I-line II AP, AF, CP, CF Busway

Cause:
Application and installation

Resolution:
Yes, the elbow fittings can be connected together without any use of transition pieces. 
Was this helpful?
What can we do to improve the information ?