Technical FAQs

Ask a Question

What is the part number for a 120V coil for a 8536SD, 8538SD, 8539SD, 8736SD, 8738SD, 8739SD type starters and 8502SD and 8702SD contactors?

Issue:
What is the part number for a 120V coil for a 8536SD type starter?

Product Line:
Starters and contactors

Environment:
NEMA class 8502 and 8536 starters and contactors

Cause:
replacement coil

Resolution:
The replacement 120V 60HZ coil part number is 31063-409-38 for 2 and 3 pole devices and 31063-400-38 for 4 and 5 pole devices. This information may be found in the current Digest or in the attached bulletin.
Was this helpful?
What can we do to improve the information ?