Technical FAQs

Ask a Question

ATV66D12N4 : How do I change Preset speeds

Issue:
How do you change the preset speed on a ATV66

Product Line:
ATV66

Environment:
All

Cause:
Preset speed adjustment

Resolution:
Go to F1 then to menu 7.2 application functions then scroll down to preset speeds, press enter and assign 1 preset speed to a logic input and assign 3 preset to another logic input, if needed. Then assign the preset speed itself.
 
Was this helpful?
What can we do to improve the information ?