Technical FAQs

Ask a Question

What is the socket part number for the 8501KUDR13 and 8501KUR13 relays?

Product Line:
Square D Universal Plug In Relays

Resolution: 
These use the same sockets as the 8501KUDR12 and 8501KUR12, which are part number 8501NR82 (sold in quantities of 1) or 8501NR82B (sold in quantities of 10).
Was this helpful?
What can we do to improve the information ?