Technical FAQs

Ask a Question

Installation of the GS1AW606 on LK4QU3N

Issue:
Which bolt kit should be used for installing the GS1AW606 on the LK4QU3N?

Product Line:
IEC Disconnect Switches - GIC Product

Environment:
US Product

Cause:
Product Installation

Resolution:
The bolt kit which is supplied with the GS1AW606 should be used for installation.  The bolt head should be installed on the back pan side of the switch and the nuts should be installed on the front.
 
Was this helpful?
What can we do to improve the information ?