Technical FAQs

Ask a Question

How many circuit breakers can be daisy chained to an IFE ethernet gateway?

Product Line:
Circuit breakers on a single modbus network

Resolution:
You can connect up to 13 breakers to one IFE/Gateway.  One connects directly to the IFE, the other 12 breakers connect to IFM modules which are daisy-chained to the IFE.  Use line terminator for any unused ports.
 
Was this helpful?
What can we do to improve the information ?