Technical FAQs

Ask a Question

Can the QO124L125GRB main lug load center be converted to a main breaker?

Issue:
Product Feature

Product Line:
QO Load centers

Environment:
Main lug to Main Breaker

Cause:
Application

Resolution:
Yes, as the current digest shows the QO124L125GRB is a convertible mains load center and uses the QOM1 Main Breaker Frame Size. So any of the QOM1 ampere rating main breakers can be ordered and used, SEE DIGEST FOR QOM1 CATALOG NUMBERS.
Was this helpful?
What can we do to improve the information ?