Technical FAQs

Ask a Question

Can you put a 15 HP ATV212 drive into a 10 HP S-Flex enclosure without modifying components and wiring?

Issue:
Can you put a 15HP drive into a 10HP drive Sflex enclosure without modifying components and wiring?

Product Line:
ATV212

Environment:
S-Flex

Cause:
Compatibility of a 15HP in a 10HP Sflex Enclosure

Resolution:
No, you cant just put a 15 HP ATV212 drive in the S-Flex 10 HP enclosure. The power wire changes from #12 to #10, the contactors change from LC1D25G7 to LC1D32G7 and the overload changes from LRD21 to LRD22.
Was this helpful?
What can we do to improve the information ?