Technical FAQs

Ask a Question

Can you adjust an IG6 LIM to 4.8ma?

Issue:
In what current or milliamp increments can you adjust the Line Isolation Monitor (LIM)?

Product Line:
Medical products LIM

Environment:
Iso Guard IG6

Cause:
 THC or current adjustments

Resolution:
The total hazard current (THC) of the IG6 can be adjusted for 2ma or 5ma. There are no in between increments. Also, there is not any exting NEC or UL code that specifies there must be an adjustment for 4.8ma. 
Was this helpful?
What can we do to improve the information ?