Technical FAQs

Ask a Question

Are there UL ratings for keypad remote mounting kit VW3A1102

Issue:
Are there UL ratings for keypad mounting kit VW3A1102

Product Line:
ATV61, ATV71, ATV212, ATV312, ATV32

Environment:
All models and serial numbers

Cause:
UL ratings for keypad enclosure

Resolution:
There are no UL certification for Extra Low Voltage options because operating voltage is less than 50V.
 

 
Was this helpful?
What can we do to improve the information ?