Technical FAQs

Ask a Question

What's the maximum permissible cable length for BCH2 motor?

Issue:
What's the maximum permissible cable length for BCH2 motor?

Product:
BCH2

Resolution:
The maximum servo motor cable length conforming to IEC/EN 61800-3 Category C3 is 20 m (65.62 ft).
This applies to both the motor cable and the encoder cable between the LXM28 drive and the BCH2 motor.
Was this helpful?
What can we do to improve the information ?