Technical FAQs

Ask a Question

What is the temperature compensation range for my MPPT charge controller?

Issue:
What is the temperature compensation range for my MPPT charge controller?

Product Line:
Conext MPPT60-150 or MPPT80-600

Environment:
MPPT installation with possible extreme temperatures

Cause:
Issue not addressed in product documentation

Resolution:
The temperature range where compensation is applied is between 0°C and 50°C. Outside of this temperature range, the compensation value is clamped at the corresponding value for either 0°C or 50°C.
Was this helpful?
What can we do to improve the information ?