Technical FAQs

Ask a Question

Instead of an Active Front End what are the options for reduced harmonics offered?

The Passive Filter and 18 Pulse units are available with increase costs of 25% and 40%, respectively.
 
Was this helpful?
What can we do to improve the information ?