Technical FAQs

Ask a Question

What are the replacement modules for a FI8IMA12C1?

Product Line:
Surge Protective Devices (SPDs)

Environment:
Generally, when the TVSS unit is inoperable, it is necessary to determine if a module can be replaced or the entire unit must be replaced.

Cause:
Maintenance

Resolution:
The replacement modules for A, B, or C phase is MA8IMA121 (one module for each phase).
Was this helpful?
What can we do to improve the information ?