Technical FAQs

Ask a Question

How to limit power output on XC\XCNA inverters?

Issue:
Need to limit the total KWatts that an inverter can produce.

Product Line:
XC or XCNA

Environment:

Causes:
Troubleshooting or requirement from the utility company.

Resolution:
1. At the display, hit the enter button by press on the turning wheel.
2. Go to Grid setting and press enter.
3. Go to Grid support option and press enter.
4. Go to User active power limit and press enter. 
5. Change the value by turning the wheel. 
6. Once it is the value you want then press enter.
7. Press the F4 button to get out.
8. The kwatt output should now be limited to the value that was changed.
 
Was this helpful?
What can we do to improve the information ?