Technical FAQs

Ask a Question

How to limit power output on the GT inverters?

Issue:
Customer wanted to limit the inverter power output

Product Line:
GT Series

Environment:

Causes:
For troubleshooting or due to utility requirement for the site.

Resolution:
1. Turn the enable\disable off
2. Go to the keypad and press the Menu button
3. Press enter button and the display will ask for password.
4. Enter the password, which is 594 and press the enter button once.
5. Press the up arrow on the keypad until you see IPPT % Max
6. The IPPT % Max Iis normally set at 100. Press enter and put in the appropriate value then press enter to accept the change.
7. Press the Menu botton once the change was made. 
8. Turn the enable\disable switch to enable and you will see that the power production is now less than before.
Was this helpful?
What can we do to improve the information ?