Technical FAQs

Ask a Question

Can the QO112M100 Convertible Mains load center be ordered with a 80A main breaker, instead of a 100A?

Issue:
Product Design features

Product Line:
QO Load Centers

Environment:
Main breaker

Cause:
Application

Resolution:
Yes, the catalog number QO112M10080 can be ordered.


 
Was this helpful?
What can we do to improve the information ?