Technical FAQs

Ask a Question

​What are the dimensions of the mounting bracket for the GT and TX model?

Issue:
Mounting bracket dimensions for the GT and TX

Product Line:
TX and GT single phase grid tie inverter

Environment:
Applications where the TX and or GT are used

Cause:
Dimension differences of the mounting brackets between the GT and TX.

Resolution:
Below is an image of the mounting bracket differences

Was this helpful?
What can we do to improve the information ?