Technical FAQs

Ask a Question

​What are the minimum clearances for the grid tie inverter?

Issue:
Clearance space above and on the sides of the unit

Product Line:
TX, GT

Environment:
Applications where a TX or GT are installed

Cause:
Clearance requirement

Resolution:
The unit should have 12 ‘’ of clearance above and 6” along the sides.  Please note if using multiple units they can be installed alongside each other but the units at the end must meet the side space requirement of 6 ‘’
Was this helpful?
What can we do to improve the information ?