Technical FAQs

Ask a Question

​What are the physical dimension differences between the TX and GT grid tie inverter?

Issue:
Physical comparison between the GT and TX

Product Line:
GT/TX grid tie single phase inverter

Environment:
Applications that use a GT or TX Grid Tie inverter

Cause:
In replacing a unit it may require knowing dimensions to see if it can be installed in a specific area

Resolution:
Below is the physical comparison between the GT and TX model grid tie inverter

Was this helpful?
What can we do to improve the information ?