Technical FAQs

Ask a Question

How do you set up the S-flex drive to run a fixed speed of 30hz?

Issue:
How do you set up the S-flex to run a fixed speed of 30hz?

Product Line:
ATV212 and S-flex enclosed 

Environment:
All 

Cause:
Wants to start the drive and have it ramp up to 30hz 

Resolution:

We made the following programming changes

FNOD= changed from 4 to 1  VIA input
CNOD= changed from 2 to 1 keypad control.

LL set from 0 to 30hz
UL set from 60 to 30hz

F---- enter
F108 set to 48

 

Was this helpful?
What can we do to improve the information ?