Technical FAQs

Ask a Question

What can I do if I am missing the mounting bracket for the XW+ 6848?

Issue
Lost/missing mounting bracket for the Conext XW/XW+/PDP

Product Line
Conext XW+, Conext Power Distribution Panel

Environment
Request for a new mounting bracket from a Conext XW+ or Conext PDP+

Cause
The bracket was lost or missing from the shipment

Resolution
The part number is 0J-0383.  This item is available through inTouch.  It cannot be ordered through Solar Order Desk.  If the unit missing the bracket is also under warranty, please contact Solar Technical Support at 866-519-1470.
Was this helpful?
What can we do to improve the information ?