Technical FAQs

Ask a Question

Can the ATV212 drive be controlled with a pulse train input signal?

Issue: 
Can the ATV212 drive be controlled with a pulse train input signal?

Product Line:
ATV212/SFlex

Environment: 
All

Cause: 
Compatibility of ATV212 to interface pulse width modulation input.

Resolution: 
The ATV212 is not compatible with pulse train input. 






 
Was this helpful?
What can we do to improve the information ?