Technical FAQs

Ask a Question

Will changing the Display Hold slow down the scroll speed in my MPPT 60 150?

Issue
The customer would like to change the amount time the MPPT60 holds on a screen before switching to the next screen.

Product Line
MPPT 60 150

Environment
Using the display of the MPPT 60 150 to read information

Cause
The amount of time the MPPT holds on screen is too short

Resolution
The scroll time is set to 4 seconds.  Unfortunately, it is not configurable.  The Display Hold is not related to the scroll time.  Instead, the Display Hold is the amount of time needed without input for the MPPT 60 display to return to the home screen.
Was this helpful?
What can we do to improve the information ?