Technical FAQs

Ask a Question

How do I recover logs from the Conext CL?

Issue
What is the process to recover service and/or energy logs from the Conext CL?

Product Line
Conext CL

Environment
Looking to download history of production and service logs from the Conext CL.

Cause
The service logs are especially useful in case of any failure.  Energy logs can be used by the customer to see their production over time.

Resolution
Make sure to have a USB flash drive available.  Size does not matter.  To avoid any unnecessary procedure, make sure that there is no firmware loaded on the USB drive.  Starting with the unit powered on.  Follow the steps below:
-Insert USB drive into USB port of Conext CL
-Press the Home button
-Select Maintenance from the menu
-The unit will request the password.  That is  1 2 3 4.
-Select "Copy Logs to USB"
-Screen will confirm when copy is completed.
-Remove USB
Was this helpful?
What can we do to improve the information ?