Technical FAQs

Ask a Question

What is the maximum number of Conext SW inverter that can be stacked together?

Issue:
Customers want to confirm the maximum number of stacked Conext SW inverters in parallel

Product Line:
Conext SW 4024 Conext SW 2524 Conext SW 4048 

Environment:
Product Information 

Causes: 

Resolution:
The Conext SW interverter have a maximum of 2 units, stacked in parallel 

 
Was this helpful?
What can we do to improve the information ?