Technical FAQs

Ask a Question

What is the data usage rate of the Conext Combox?

Issue
What is the data usage rate for the Combox when it pushes data to Conext Insight

Product Line
Conext Combox, Conext Insight

Environment
Combox connected via internet to a Conext Insight Account

Cause
Some customers have strict data limits, so it is important to know how much data to budget for the Insight connection.  If the customer uses a wireless/mobile connection, then they can figure out how large of a data plan would be needed.

Resolution
Results will vary depending on the size of the actual system.  A system with 2 XW 6048 and 2 MPPT 60 150 generates a packet file averaging 2.5kB.  Assuming there is a reliable internet connection, the Combox will push to Conext Insight every 10 minutes or 6 times an hour.  

2.5kB x 6 pushes per hour x 24 hours x 30 days is roughly equal to 11MB per month.

The amount will vary proportionally to the amount of devices on the Xanbus network, but the result is a relatively small amount of data.
Was this helpful?
What can we do to improve the information ?