Technical FAQs

Ask a Question

What drives are compatible with the VW3A1111 keypad display?

Issue:
Is the VW3A1111 Graphic keypad compatible with the ATV320?
 
Product Line:
ATV320
 
Environment:
ALL
 
Cause:
Compatibility with the 320 drive

 
Resolution:
Enhanced graphic display is only compatible with these drives:
 
Range compatibility Altivar 212
Altivar 32
Altivar Process ATV600
Altivar Machine ATV340
Altivar Lift
Altivar 312 Solar
Altivar 61Q
Altivar Easy 610
Altivar Process ATV900
Lexium 32
Altivar 71Q
Altivar 312
Altivar 71
Altivar Machine ATV320
Altivar 61  
Was this helpful?
What can we do to improve the information ?