Technical FAQs

Ask a Question

What is the maximum number of auxiliary contacts on a NEMA Size 4 Starter?

Product Line:
NEMA Type S Starters

Resolution: 
3 Auxiliary Contacts as well as the existing Holding Contact.
Was this helpful?
What can we do to improve the information ?