Technical FAQs

Ask a Question

Are the ATV630/930 drives 8 series compatible?

Issue: 
Are the ATV630/930 drives 8 series compatible?

Product Line:
ATV630/930 Series

Environment:
ALL

Cause:
The ATV61 had a series 8 mode that would mimic the memory map of an ATV58

Resolution: 
Currently the ATV630/930 process drives are not capable of 8 series mode like the ATV61 drives. 
Was this helpful?
What can we do to improve the information ?