Technical FAQs

Ask a Question

What is the heat sink cooling fan part number for the ATV21 and ATV212 drives?

Issue:
What is the heat sink cooling fan part number for the ATV21 and ATV212 drives?

Product Line:
Altivar ATV21, ATV212,S-Flex 21 and S-Flex 212

Environment:
All

Cause:
Needs a replacement cooling fan for the ATV21 and ATV212 drives

Resolution:
See the attached file 
Was this helpful?
What can we do to improve the information ?