Technical FAQs

Ask a Question

Can I save PDFs on the SD card of a TM241 and view them in a web visualization?

Issue:
Can I save PDFs on the SD card of a TM241 and view them in a web visualization?

Product Line:
TM241

Resolution:
Today, it is not possible to show a PDF document in web visualization. 
With SoMachine V5, it will be possible to add a hyperlink to a visualization which navigates to external webpages and also to documents stored on the internal file system (and SD card). 
Was this helpful?
What can we do to improve the information ?