Technical FAQs

Ask a Question

What is the torque requirement for Alarm Switch (SD), Overcurrent Trip Switch (SDE) and Auxiliary Switch (OF) Kits for PowerPact™ H-, J-, L-, M-, P-, and R-Frame, and NS630b–NS3200 Circuit Breakers?

Answer
Issue:
Torque Requirements on Molded case circuit breaker accessories

Product Line:
Powerpact Circuit Breakers

Environment:
Accessories

Cause:
Installation

Resolution:

The torque requirement is 10 lb-in. May need torque screw to measure this low torque.

Keywords,

torque, S29450, LV426950, LV426951, LV426952, S29451, S29452, S33801
Was this helpful?
What can we do to improve the information ?