Technical FAQs

Ask a Question

What main breaker is used in the CQO160M200CPON and can a lower amperage main be installed?

Issue:
Product Design Features

Product Line:
Canadian QO Load Centers

Environment:
Main Breaker

Cause:
Application

Resolution:
The main breaker used in this load center is the QOM2 Frame Size and below is a list of the main breakers that can be used in this load center.
1) Factory installed Main Breaker - QOM2200VHL
2) 100amp Main breaker - QOM2100VHL
3) 125amp Main breaker - QO2125VHL
4) 150amp Main breaker - QOM2150VHL
5) 175amp Main Breaker - QOM2175VHL

 
Was this helpful?
What can we do to improve the information ?