Technical FAQs

Ask a Question

Where can I get the minimum resistance and braking resistors for the Altivar 930 and Altivar 950 drives?

Issue:
Where can I get the minimum resistance and braking resistors for the Altivar 930 and Altivar 950 drives?

Product Line:
Altivar 930 and Altivar 950 drives

Environment:
Altivar 930 and Altivar 950 drives

Cause:
Min braking resistance to add a Dynamic Braking Resistor

Resolution:
Attached is the spreadsheet that shows all the minimum resistance value of the ATV930 drives.
Was this helpful?
What can we do to improve the information ?