Technical FAQs

Ask a Question

Looking for the CN10 connector on the LXM32 drive.

Issue:
Looking for the CN10 connector on the LXM32 drive

Product Line:
LXM32

Resolution:
The CN10 connector on the LXM32 drive cannot be sold alone.
It comes in a complete connectors kit, part# VW3M2202. This kit is included in the box when buying a LXM32 drive and can be ordered separately.
Was this helpful?
What can we do to improve the information ?