Technical FAQs

Ask a Question

What is an HQ23186R?

Product Line 
HQ2 Load Centers

Resolution:
The HQ2/318-6R  panel, which is now obsolete, was an I-line construction device rated 1P3W, 120/240V. The branch breakers used were of the I-line construction types Q2 and FA breakers type, with BC phasing ONLY.  Since the Q2 breakers are now obsolete, the Powerpact Q I-line breakers with suffix "4" can be used in their place.
Was this helpful?
What can we do to improve the information ?