Technical FAQs

Ask a Question

Does the ELM fit inside of the breaker, or does it attach to the end and make the breaker longer?

Product Line;
ELM Earth Leakage Module

Resolution;
The ELM does not fit inside of the breaker. It attaches to the load end, therefore adding about 4" to the total length of the breaker.
 
Was this helpful?
What can we do to improve the information ?