Technical FAQs

Ask a Question

Is a RIM module restrained when it is not powered?

Issue:
Is a RIM module restrained when it is not powered?

Product Line:
Micrologic trip unit accessories

Environment:
Molded Case Circuit Breakers

Cause:
Product Characteristics

Resolution:
The RIM module will default to the maintenance mode when not powered. The RIM module must be powered to allow normal breaker tripping.
Was this helpful?
What can we do to improve the information ?