Technical FAQs

Ask a Question

How to clear fault on the PV Series inverters PV10,PV 20, PV30 and PV45?

Issue:
Inverter faulted and would not run

Product Line:
PV Series inverters (Prior to PV100s)

Environment:

Cause:
Unknown, not true or been resolved

Resolution:
Unlike later model of inverter that has the keypad on the display, older model does not. Therefore, it does not have a feature to clear fault by pressing the F1 button.
However, one can do a similar trick by turn the ON\OFF switch to off and on and off and on really quick and the fault will clear. 
 
Was this helpful?
What can we do to improve the information ?