Technical FAQs

Ask a Question

Does the ATV61 and ATV71 come with Ethernet as a standard protocol?

Issue:
Does the ATV61 and ATV71 come with Ethernet as a standard protocol?

Product Line:
Altivar ATV61 and ATV71 drives

Environment:
All 

Cause:
Is Ethernet standard on the ATV61 and ATV71 drives?

Resolution:
ATV61 and ATV71 drives do not come with Ethernet as a standard protocol.  If you need the option card you can order the VW3A3320 combo Ethernet TCP-IP and  IP option card.
A second option would be the VW3A3310D standard Ethernet TCP-IP card or the VW3A3316 standard Ethernet IP option card. 
Was this helpful?
What can we do to improve the information ?