Technical FAQs

Ask a Question

Why is there no display on the GKP for an XCNA?

Issue: 
There is nothing displayed on the GKP even though the QS2 (control power) is turned on.

Product Line:
XCNA

Environment:

Cause:
Possible loose connection or something is tripped.

Resolution:
There is a RJ45 cable that connects from the GKP to the CMX board. Make sure to check the cable for damages or check the connection at both places. Check the 24 and 48 VDC power supplies to see if there is power coming in and out. If there is no LED on them, check the QF2. It might be tripped.
Was this helpful?
What can we do to improve the information ?