Technical FAQs

Ask a Question

What is the Fan strategy on ATV 61 Plus 800hp drive?

Issue: 
Can I turn off the fan when the drive is not running?

Product Line: 
ATV61 Plus 

Environment:
800hp  

Cause:

Can I turn off the fan when the drive is not running?

Resolution:
The fans runs when the run command is given or when the drive thermal is greater than or equal to 70% and turns off when the drive thermal is less than 60% and runs for 10 minutes after the run command is removed.
There is no internal parameter to change this fan management.
 
Was this helpful?
What can we do to improve the information ?